SF_TestableSafetySensorPermalink

This is the web edition of the original ‎⮫ AC500-S safety user manual, version 1.3.2. This web edition is provided for quick reference only. The original safety user manual must be used to meet functional safety application requirements.

Standards

Requirements

IEC 61496-1:2012

4.2.2.3 Particular requirements for a type 2 ESPE

A type 2 ESPE shall have an means of periodic test to reveal a failure to danger (for example, loss of detection capability, response time exceeding that specified).

The test shall be performed at power-on of the ESPE before going to the ON state and at each reset as a minimum.

Note: Depending on the application, the periodic test may need to be performed more often to achieve a desired safety performance.

A single fault resulting in the loss of detection capability or the increase in response time beyond the specified time or preventing one or more of the OSSDs going to the OFF state, shall result in a lock-out condition as a result of the next periodic test.

Where the periodic test is intended to be initiated by an external (for example, machine) safety-related control system, the ESPE shall be provided with suitable input facilities (for example, terminals).

The duration of the periodic test shall be such that the intended safety function is not impaired.

Note: If the type 2 ESPE is intended for use as a trip device (for example, when used as a perimeter guard), and the duration of the periodic test is greater than 150 ms, it is possible for a person to pass through the detection zone without being detected. In this case, a restart interlock should be included.

If the periodic test is automatically initiated, the correct functioning of the periodic test shall be monitored. In the event of a fault, the OSSD(s) shall be signalled to go to the OFF state.

If one or more OSSDs do not go to the OFF state, a lock-out condition shall be initiated.

An ESPE with only one OSSD shall have a minimum of one SSD (see clause A.4).

ISO 13849-1:2015

5.2.2 Manual reset function

ISO 12100-2:2010

6.2.11.4: Restart following power failure/spontaneous restart

SF_TestableSafetySensor

This function block detects, for example, the loss of the sensing unit detection capability, the response time exceeding that specified, and static ON signal in single-channel sensor systems. It can be used for external testable safety sensors (ESPE: electro-sensitive protective equipment, such as a light beam).

Table 1087: FB name: SF_TestableSafetySensor

Name

Data type

Initial value

Description, parameter values

VAR_INPUT

Activate

BOOL

FALSE

⮫ Table 1055 “General input parameters”

S_OSSD_In

BOOL

FALSE

Variable.

Status of sensor output, e.g., light curtain.

FALSE: Safety sensor in test state or demand for safety-related response.

TRUE: Sensor in the state for normal operating conditions.

StartTest

BOOL

FALSE

Variable.

Input to start sensor test. Sets "S_TestOut" and starts the internal time monitoring function in the FB.

FALSE: No test requested.

TRUE: Test requested.

NoExternalTest

BOOL

FALSE

Constant.

Indicates if external manual sensor test is supported.

FALSE: The external manual sensor test is supported. Only after a complete manual sensor switching sequence, an automatic test is possible again after a faulty automatic sensor test.

TRUE: The external manual sensor test is not supported.

An automatic test is possible again without a manual sensor switching sequence after faulty automatic sensor test.

S_StartReset

BOOL

FALSE

⮫ Table 1055 “General input parameters”

S_AutoReset

BOOL

FALSE

⮫ Table 1055 “General input parameters”

Reset

BOOL

FALSE

⮫ Table 1055 “General input parameters”

TestTime

TIME

T#10ms

Constant. Range: 0 ... 150ms.

Test time of safety sensor.

VAR_OUTPUT

Ready

BOOL

FALSE

⮫ Table 1056 “General output parameters”

S_OSSD_Out

BOOL

FALSE

Safety related output indicating the status of the ESPE.

FALSE: The sensor has a safety-related action request or test error.

TRUE: The sensor has no safety-related action request and no test error.

S_TestOut

BOOL

TRUE

Coupled with the test input of the sensor.

FALSE: Test request issued.

TRUE: No test request.

TestPossible

BOOL

FALSE

Feedback signal to the process.

FALSE: An automatic sensor test is not possible.

TRUE: An automatic sensor test is possible.

TestExecuted

BOOL

FALSE

A positive signal edge indicates the successful execution of the automatic sensor test.

FALSE:

  • An automatic sensor test was not executed yet.

  • An automatic sensor test is active.

  • An automatic sensor test was faulty.

TRUE: A sensor test was executed successfully.

SafetyDemand

BOOL

FALSE

Optional.

⮫ Table 1056 “General output parameters”

ResetRequest

BOOL

FALSE

Optional.

⮫ Table 1056 “General output parameters”

Error

BOOL

FALSE

⮫ Table 1056 “General output parameters”

DiagCode

WORD

16#0000

⮫ Table 1056 “General output parameters”

Typical timing diagram

Fig. 494: Typical timing diagram for SF_TestableSafetySensor

SF_TestableSafetySensor_TimingDiagram

Error detection

The following conditions force a transition to the error state:

  • Test time overrun without delayed sensor feedback.

  • Test without sensor signal feedback.

  • Invalid static reset signal in the process.

  • Plausibility check of the monitoring time setting.

Error behavior

In the event of an error, the S_OSSD_Out output is set to FALSE and remains in this safe state.

Once the error has been removed and the sensor is on (S_OSSD_In = TRUE) - a reset removes the error state and sets the S_OSSD_Out output to TRUE.

If S_AutoReset = FALSE, a rising trigger is required at Reset.

After transition of S_OSSD_In to TRUE, the optional startup inhibit can be reset by a rising edge at the Reset input.

After block activation, the optional startup inhibit can be reset by a rising edge at the Reset input.

Function block-specific error and status codes

Table 1088: FB-specific error codes

DiagCode

State name

State description and output setting

C000

Parameter Error

Invalid value at the TestTime parameter.

Values between 0 ms and 150 ms are possible.

Ready = TRUE

S_OSSD_Out = FALSE

S_TestOut = TRUE

TestPossible = FALSE

TestExecuted = FALSE

SafetyDemand = FALSE

ResetRequest = FALSE

Error = TRUE

C001

Reset Error 1

Static Reset condition detected after FB activation.

Ready = TRUE

S_OSSD_Out = FALSE

S_TestOut = TRUE

TestPossible = FALSE

TestExecuted = FALSE

SafetyDemand = FALSE

ResetRequest = FALSE

Error = TRUE

C011

Reset Error 2

Static Reset condition detected in state 8402.

Ready = TRUE

S_OSSD_Out = FALSE

S_TestOut = TRUE

TestPossible = FALSE

TestExecuted = FALSE

SafetyDemand = FALSE

ResetRequest = FALSE

Error = TRUE

C021

Reset Error 3

Static Reset condition detected in state Cx10.

Ready = TRUE

S_OSSD_Out = FALSE

S_TestOut = TRUE

TestPossible = FALSE

TestExecuted = FALSE

SafetyDemand = FALSE

ResetRequest = FALSE

Error = TRUE

C031

Reset Error 4

Static Reset condition detected in state 8404.

Ready = TRUE

S_OSSD_Out = FALSE

S_TestOut = TRUE

TestPossible = FALSE

TestExecuted = FALSE

SafetyDemand = FALSE

ResetRequest = FALSE

Error = TRUE

C041

Reset Error 5

Static Reset condition detected in state C000.

Ready = TRUE

S_OSSD_Out = FALSE

S_TestOut = TRUE

TestPossible = FALSE

TestExecuted = FALSE

SafetyDemand = FALSE

ResetRequest = FALSE

Error = TRUE

C051

Reset Error 6

Static Reset condition detected in state 8406.

Ready = TRUE

S_OSSD_Out = FALSE

S_TestOut = TRUE

TestPossible = FALSE

TestExecuted = TRUE

SafetyDemand = FALSE

ResetRequest = FALSE

Error = TRUE

Cx10

Test Error 1

Test time elapsed in state 8020 or 8030.

IF S_OSSD_IN = TRUE AND NoExternalTest = TRUE THEN x = 4

ELSE x = 0;

Output signals for x = 4 (C410):

Ready = TRUE

S_OSSD_Out = FALSE

S_TestOut = TRUE

TestPossible = FALSE

TestExecuted = FALSE

SafetyDemand = FALSE

ResetRequest = TRUE

Error = TRUE

Output signals for x = 0 (C010):

Ready = TRUE

S_OSSD_Out = FALSE

S_TestOut = TRUE

TestPossible = FALSE

TestExecuted = FALSE

SafetyDemand = FALSE

ResetRequest = FALSE

Error = TRUE

Table 1089: FB-specific status codes (no error):

DiagCode

State name

State description and output setting

0000

Idle

The function block is not active (initial state).

Ready = FALSE

S_OSSD_Out = FALSE

S_TestOut = TRUE

TestPossible = FALSE

TestExecuted = FALSE

SafetyDemand = FALSE

ResetRequest = FALSE

Error = FALSE

8401

Init

An activation has been detected by the FB.

Ready = TRUE

S_OSSD_Out = FALSE

S_TestOut = TRUE

TestPossible = FALSE

TestExecuted = FALSE

SafetyDemand = FALSE

ResetRequest = TRUE

Error = FALSE

8802

ESPE Interrupted 1

The FB has detected a safety demand.

The switch has not been automatically tested yet.

Ready = TRUE

S_OSSD_Out = FALSE

S_TestOut = TRUE

TestPossible = FALSE

TestExecuted = FALSE

SafetyDemand = TRUE

ResetRequest = FALSE

Error = FALSE

8402

Wait for Reset 1

Wait for rising trigger of Reset after state 8802.

Ready = TRUE

S_OSSD_Out = FALSE

S_TestOut = TRUE

TestPossible = FALSE

TestExecuted = FALSE

SafetyDemand = FALSE

ResetRequest = TRUE

Error = FALSE

8002

External Function Test

The automatic sensor test was faulty.

An external manual sensor test is necessary.

The support for the necessary external manual sensor test has been activated at the FB (NoExternalTest = FALSE).

A negative signal edge at the sensor is required.

Ready = TRUE

S_OSSD_Out = FALSE

S_TestOut = TRUE

TestPossible = FALSE

TestExecuted = FALSE

SafetyDemand = FALSE

ResetRequest = FALSE

Error = FALSE

8804

ESPE Interrupted External Test

The automatic sensor test was faulty.

An external manual sensor test is necessary.

The support for the necessary external manual sensor test has been activated at the FB (NoExternalTest = FALSE).

A TRUE signal at the sensor is required.

Ready = TRUE

S_OSSD_Out = FALSE

S_TestOut = TRUE

TestPossible = FALSE

TestExecuted = FALSE

SafetyDemand = TRUE

ResetRequest = FALSE

Error = FALSE

8404

End External Test

The automatic sensor test was faulty.

An external manual sensor test is necessary.

The support for the necessary external manual sensor test has been activated at the FB (NoExternalTest = FALSE).

The external manual test is complete.

The FB detected a complete sensor switching cycle (externally controlled).

Ready = TRUE

S_OSSD_Out = FALSE

S_TestOut = TRUE

TestPossible = FALSE

TestExecuted = FALSE

SafetyDemand = FALSE

ResetRequest = TRUE

Error = FALSE

8010

ESPE Free No Test

The FB has not detected a safety demand.

The sensor has not been tested automatically.

Ready = TRUE

S_OSSD_Out = TRUE

S_TestOut = TRUE

TestPossible = TRUE

TestExecuted = FALSE

SafetyDemand = FALSE

ResetRequest = FALSE

Error = FALSE

8806

ESPE Interrupted 2

The FB has detected a safety demand.

The switch was automatically tested.

Ready = TRUE

S_OSSD_Out = FALSE

S_TestOut = TRUE

TestPossible = FALSE

TestExecuted = TRUE

SafetyDemand = TRUE

ResetRequest = FALSE

Error = FALSE

8406

Wait for Reset 2

Wait for rising trigger of Reset after state 8806.

Ready = TRUE

S_OSSD_Out = FALSE

S_TestOut = TRUE

TestPossible = FALSE

TestExecuted = TRUE

SafetyDemand = FALSE

ResetRequest = TRUE

Error = FALSE

8020

Test Request

The automatic sensor test is active. Test Timer is started first time.

The transmitter signal of the sensor is switched off by the FB.

The signal of the receiver must follow the signal of the transmitter.

Ready = TRUE

S_OSSD_Out = TRUE

S_TestOut = FALSE

TestPossible = FALSE

TestExecuted = FALSE

SafetyDemand = FALSE

ResetRequest = FALSE

Error = FALSE

8030

Test Active

The automatic sensor test is active. Test Timer is started second time. Timer 1 is stopped.

The transmitter signal of the sensor is switched on by the FB.

The signal of the receiver must follow the signal of the transmitter.

Ready = TRUE

S_OSSD_Out = TRUE

S_TestOut = TRUE

TestPossible = FALSE

TestExecuted = FALSE

SafetyDemand = FALSE

ResetRequest = FALSE

Error = FALSE

8000

ESPE Free Test ok

The FB has not detected a safety demand. Timer 2 is stopped.

The sensor was automatically tested.

Ready = TRUE

S_OSSD_Out = TRUE

S_TestOut = TRUE

TestPossible = TRUE

TestExecuted = TRUE

SafetyDemand = FALSE

ResetRequest = FALSE

Error = FALSE